VM.ERR
Description
Determine the particular problem causing Runtime Error (F4 Fault) by looking at the value of the VM.ERR variable. Use the Variables Window to find the value of VM.ERR.
The table below shows what each value of VM.ERR means.
Value of VM.ERR | Error Caused by: |
---|---|
801 | Divide by zero. |
802 | Stack overflow. |
803 | Insufficient memory. |
804 | No interrupt handler defined. |
805 | Interrupt error. |
806 | Max string length exceeded. |
807 | String overflow. |
808 | Array out of bounds |
809 | Feature not supported. |
810 | Internal firmware/hardware error. |
812 | Parameter not supported. |
813 | Parameter access error. |
814 | Data not found. |
815 | Data invalid. |
816 | Data too high. |
817 | Data too low. |
818 | Param type out of range. |
819 | Data not divisible by 2. |
820 | Invalid position modulo setting. |
821 | Cannot read from command. |
823 | Enable Drive first. |
824 | DRV.OPMODE must be 2 (position). |
825 | DRV.CMDSOURCE must be 5 (program). |
826 | Cannot execute during a move. |
827 | Writing to read-only parameter. |
828 | Disable Drive first. |
General Information
Type |
R/W |
Units |
None |
Range |
0 to 1000 |
Default Value |
0 |
Data Type |
Integer |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
---|---|---|---|---|---|
Modbus |
1162 |
No | 32 bit | No |
M_01-05-11-000 |